# Deployment > *❗Important: The library/binary generated by eIQ Time Series Studio is licensed exclusively for use on NXP devices. It must be implemented and deployed solely on NXP products.* After completing [Emulation](Emulation.md) and identifying the optimal model, switch to the **“Deployment”** tab to generate and deploy the optimized algorithm. The Deployment process generates **the optimized algorithm library or binary along with a sample project**, which can then be offloaded to edge devices. The Deployment section represents the **final** stage of the pipeline. It provides step-by-step guidance to generate and deploy the algorithm for your project on target devices. > *Notes: Deployment requires public network support because the Cloud Server dynamically generates target libraries or binaries specific to your CPU, model, and IDE.* -------------------- ## Function Layout ![alt text](_static/picture/deployment/dep_function_layout.jpg) The Deployment section of eIQ Time Series Studio supports the following main functions: - [Optional Algorithm Formats](#supported-algorithm-formats). - [Multiple Compilers](#supported-compilers). - [Multiple Target Architectures](#supported-architectures). - [Arm Cortex-M Compilation Flags](#supported-compilation-flags). - [Hardware Accelerator Options](#supported-accelerator-options). - [Multi-Library Generation](#multi-library-generation). - [Step-by-Step Deployment Instructions](#deployment-process). - [Cloud-Based Algorithm Integration](#algorithm-integration). - [QuickStart Sample Project (MCUXpresso)](#algorithm-project-execution). ## Supported Algorithm Formats The final deliverable of the algorithm supports two optional formats: - **Library(*.a or *.lib):** Updating the algorithm requires relinking and rebuilding the entire firmware project. - **Binary(*.bin):** The algorithm can be updated independently by updating only the corresponding firmware section, without requiring a full firmware upgrade. > *Notes: Currently, the binary format is supported only on the **FRDM‑MCXN947** target. Support for more targets will be added in future releases.* ## Supported Compilers eIQ Time Series Studio supports the following compilers: - **GCC** (MCUXpresso, GNU ARM Embedded Toolchain) - **Arm Compiler** (Keil MDK) - **IAR Compiler** (IAR Embedded Workbench For Arm) ![alt text](_static/picture/deployment/dep_supported_compilers.jpg) - **CodeWarrior** (CodeWarrior Development Studio For DSC) ![alt text](_static/picture/deployment/dep_supported_compilers_CodeWarrior.jpg) ## Supported Architectures - **Arm Cortex-M series** (widely used in microcontrollers) - **NXP DSC cores** (Digital Signal Controllers) - **Arm Cortex-A series** (via GCC) ## Supported Compilation Flags The supported compilation flags are: - **float-abi:** Specifies which floating-point ABI to use. (hard/soft). Default: `hard`. - **fshort-wchar:** Sets the size of wchar_t. Default: `-fno-short-wchar`. - **fshort-enums:** Sets the enumeration type to the smallest data type that can hold all enumerator values. Default: `-fshort-enums` for GCC, `-fno-short-enums` for Arm Compiler. > *Notes: Reference from the [Arm Compiler Reference Guide](https://developer.arm.com/documentation/dui0774/latest/)*. ## Supported Accelerator Options - **PowerQuad DSP:** Accelerates FFT calculation. The target device must contain this hardware. - **Neutron NPU:** Accelerates deep learning model predictions. The target device must contain this hardware. ## Multi-Library Generation **Multi-Library** enables users to link multiple TSS libraries within the same project or device, allowing each library to operate independently. In industrial and home appliance applications, projects often integrate multiple sensor types and models that **simultaneously** provide independent time series data at different sampling rates. The **Multi-Library** feature enables users to deploy dedicated TSS libraries for each independent set of time series data. Each library can incorporate different algorithm types, such as Anomaly Detection, Classification, or Regression. The inference results can be processed independently or combined to support higher-level, systemwide decision-making. ![alt text](_static/picture/deployment/dep_multi_library.jpg) Libraries are differentiated by **customized suffix names in the Deployment** section. The suffix is applied consistently to the library filename, header filename, macro definitions, and API symbols in the header file. By invoking APIs with distinct suffix names, the application can explicitly select the corresponding TSS library, enabling multiple libraries to coexist within the same project without naming conflicts. > *Notes: The generation of sample projects is not supported when the Multi-Library generation is enabled*. -------------------- ## Deployment Process ### Library Format Deployment Steps ![alt text](_static/picture/deployment/dep_deployment_process.jpg) Follow the steps and **generate** your own time series **library** and deploy it to your devices: 1. **Select Format**: Choose `Library` as the algorithm format type. 2. **Select Model**: Pick the best quality model from the [Emulation](Emulation.md) process. 3. **Select CPU Core**: Choose the `CPU core` of the target board. 4. **Project Generation**: Decide whether to generate with a MCUXpresso project. 5. **Suffix Name**: Set library suffix for Multi-Library projects (optional). 6. **Compiler**: Choose a compiler (“CodeWarrior” for DSC core). 7. **Accelerator Options**: Configure the hardware accelerator if supported. 8. **Compilation Flags**: Select optimal flags for the compiler. 9. **Generate**: Click `GENERATE` button and create library or project from Cloud. 10. **Download**: Download and unzip the generated package. 11. **Deploy**: `Link` the library to your project or `import` the generated project to MCUXpresso IDE, `build` the project, and `flash` to the target device. ### Binary Format Deployment Steps ![alt text](_static/picture/deployment/dep_deployment_process_bin.jpg) Follow the steps and generate your own time series binary and deploy it to your devices: 1. **Select Format**: Choose `Binary` as the algorithm format type. 2. **Configure Section**: Set binary configuration parameters for deployment. Ensure that the configuration matches to the firmware project settings. ![alt text](_static/picture/deployment/dep_bin_text_ram_section.jpg) 3. **Select Model**: Pick the best quality model from the [Emulation](Emulation.md) process. 4. **Select CPU Core**: Choose the `CPU core` of the target board. 5. **Project Generation**: Decide whether to generate with a MCUXpresso project. 6. **Compiler**: Choose the compiler. Currently, only "GCC" is supported for binary format. 7. **Accelerator Options**: Configure the hardware accelerator if supported. 8. **Compilation Flags**: Select optimal flags for the compiler. 9. **Generate**: Click `GENERATE` button and create binary or project from Cloud. 10. **Download**: Download and unzip the generated package. 11. **Deploy**: `Flash` the binary to the target device in the designated algorithm firmware section. `Import` the generated project to MCUXpresso IDE to know how to use the binary in your application. #### LinkServer(inc. CMSIS-DAP) Programming Support Programming via LinkServer(inc. CMSIS-DAP) is supported. Ensure that the target board is connected to your PC through a LinkServer debugger before proceeding. 1. Refresh to list the connected LinkServer probe. 2. Select the desired LinkServer probe from the list. 3. Click `PROGRAM` and flash the binary to the target device in the designated algorithm firmware section. -------------------- ## Algorithm Integration **eIQ Time Series Studio Library/Binary** is an algorithm library or binary for edge devices. The time series cloud server dynamically generates **embedded C/C++** code and **cross-compiles** based on your specific hardware and compiler information. ![alt text](_static/picture/deployment/dep_generator_architecture.jpg) ### Generated Package Structure **Library Package**: 📦_libtss ┣ 📜algorithm.dat ┣ 📜libtss.a or tss.lib ┣ 📜LICENSE.txt ┣ 📜metadata.json ┗ 📜TimeSeries.h **Binary Package**: 📦_binary ┣ 📜algorithm.dat ┣ 📜libtss.bin ┣ 📜LICENSE.txt ┣ 📜metadata.json ┗ 📜TimeSeries.h - **algorithm.dat:** The encrypted file with the algorithm details. NXP cloud server can parse and generate the source code. - **libtss.a / tss.lib / libtss.bin:** The core algorithm library or binary; developers use it for algorithm integration. (If Arm Compiler or CodeWarrior is selected, the generated library is **tss.lib**) - **LICENSE.txt:** NXP online code hosting software license agreement. - **metadata.json:** The meta description file for the generated algorithm. The file contains key information like compiler type, task type, input dataset, and platform information. The file also contains the minimum memory size as reference. - **TimeSeries.h:** The API header file for the library or binary, developers use it for the algorithm integration. ### Sample Code Integration The documentation provides sample code examples for integrating the library or binary into your project for different task types (Anomaly detection, n-Class Classification, 1-Class Classification, and Regression). #### Sample Code For Library
Anomaly detection ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; static int algo_init() { p_tss_task_ops = tss_get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; float probability; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); assert(p_data != NULL); if (p_tss_task_ops->task == TASK_AD_ODL) { /* * It's also ok that input pre-learned knowledge stored in p_algo_attr->model_addr. * Here we use online learning to train the model with normal data samples. * Input NULL to skip pre-learned knowledge. */ status = p_tss_task_ops->ad_odl_ops.init(NULL); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } /*The learning number is customizable, but we recommend the number greater than TSS_RECOMMEND_LEARNING_SAMPLE_NUM to get better results.*/ int learning_num = p_algo_attr->recommend_learning_num; for (int i = 0; i < learning_num; i++) { sample_data(p_data); status = p_tss_task_ops->ad_odl_ops.learn(p_data); if (status != TSS_LEARNING_NOT_ENOUGH && status != TSS_RECOMMEND_LEARNING_DONE) { /* Handle the learning failure cases */ } } } else { status = p_tss_task_ops->ad_ops.init(); } if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); if (p_tss_task_ops->task == TASK_AD_ODL) { status = p_tss_task_ops->ad_odl_ops.predict(p_data, &probability); } else { status = p_tss_task_ops->ad_ops.predict(p_data, &probability); } if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
n-Class Classification ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; static int algo_init() { p_tss_task_ops = tss_get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; int class_index; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); float *p_result = (float *)malloc(p_algo_attr->target_num * sizeof(float)); assert(p_data != NULL && p_result != NULL); status = p_tss_task_ops->cls_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->cls_ops.predict(p_data, p_result, &class_index); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
1-Class Classification ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ /* Decision score indicating anomaly/outlier status. Positive values (score > 0) indicate normal samples, * while negative values suggest outliers/anomalies. is_outlier flag is derived by thresholding at 0. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; static int algo_init() { p_tss_task_ops = tss_get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; int is_outlier; float score; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); assert(p_data != NULL); status = p_tss_task_ops->oc_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->oc_ops.predict(p_data, &score, &is_outlier); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
Regression ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; static int algo_init() { p_tss_task_ops = tss_get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); float *p_targets = (float *)malloc(p_algo_attr->target_num * sizeof(float)); assert(p_data != NULL && p_targets != NULL); status = p_tss_task_ops->reg_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->reg_ops.predict(p_data, p_targets); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```

#### Sample Code For Binary
Anomaly detection ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; typedef struct tss_binary_header { char magic[8]; /* "TSS1.5.0" */ const tss_task_ops_t *(*get_task_ops)(void); } tss_binary_header_t; static int algo_init() { tss_binary_header_t* (*entry)(void); extern uint32_t __base_BINARY_FLASH; entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1); tss_binary_header_t *p_algo_head = entry(); printf("MAGIC NUMBER:"); int i = 0; for(i = 0; i < 8; i++) { printf("%c", p_algo_head->magic[i]); } p_tss_task_ops = p_algo_head->get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; float probability; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); assert(p_data != NULL); if (p_tss_task_ops->task == TASK_AD_ODL) { /* * It's also ok that input pre-learned knowledge stored in p_algo_attr->model_addr. * Here we use online learning to train the model with normal data samples. * Input NULL to skip pre-learned knowledge. */ status = p_tss_task_ops->ad_odl_ops.init(NULL); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } /*The learning number is customizable, but we recommend the number greater than TSS_RECOMMEND_LEARNING_SAMPLE_NUM to get better results.*/ int learning_num = p_algo_attr->recommend_learning_num; for (int i = 0; i < learning_num; i++) { sample_data(p_data); status = p_tss_task_ops->ad_odl_ops.learn(p_data); if (status != TSS_LEARNING_NOT_ENOUGH && status != TSS_RECOMMEND_LEARNING_DONE) { /* Handle the learning failure cases */ } } } else { status = p_tss_task_ops->ad_ops.init(); } if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); if (p_tss_task_ops->task == TASK_AD_ODL) { status = p_tss_task_ops->ad_odl_ops.predict(p_data, &probability); } else { status = p_tss_task_ops->ad_ops.predict(p_data, &probability); } if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
n-Class Classification ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; typedef struct tss_binary_header { char magic[8]; /* "TSS1.5.0" */ const tss_task_ops_t *(*get_task_ops)(void); } tss_binary_header_t; static int algo_init() { tss_binary_header_t* (*entry)(void); extern uint32_t __base_BINARY_FLASH; entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1); tss_binary_header_t *p_algo_head = entry(); printf("MAGIC NUMBER:"); int i = 0; for(i = 0; i < 8; i++) { printf("%c", p_algo_head->magic[i]); } p_tss_task_ops = p_algo_head->get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; int class_index; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); float *p_result = (float *)malloc(p_algo_attr->target_num * sizeof(float)); assert(p_data != NULL && p_result != NULL); status = p_tss_task_ops->cls_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->cls_ops.predict(p_data, p_result, &class_index); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
1-Class Classification ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ /* Decision score indicating anomaly/outlier status. Positive values (score > 0) indicate normal samples, * while negative values suggest outliers/anomalies. is_outlier flag is derived by thresholding at 0. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; typedef struct tss_binary_header { char magic[8]; /* "TSS1.5.0" */ const tss_task_ops_t *(*get_task_ops)(void); } tss_binary_header_t; static int algo_init() { tss_binary_header_t* (*entry)(void); extern uint32_t __base_BINARY_FLASH; entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1); tss_binary_header_t *p_algo_head = entry(); printf("MAGIC NUMBER:"); int i = 0; for(i = 0; i < 8; i++) { printf("%c", p_algo_head->magic[i]); } p_tss_task_ops = p_algo_head->get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { tss_status status; int is_outlier; float score; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); assert(p_data != NULL); status = p_tss_task_ops->oc_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->oc_ops.predict(p_data, &score, &is_outlier); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```
Regression ```c /* * Copyright 2024-2026 NXP * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used * strictly in accordance with the applicable license terms. By expressly accepting such terms or by * downloading, installing, activating and/or otherwise using the software, you are agreeing that you * have read, and that you agree to comply with and are bound by, such license terms. If you do not * agree to be bound by the applicable license terms, then you may not retain, install, activate or * otherwise use the software. */ #include #include #include #include #include "TimeSeries.h" static void sample_data(float data_buffer[]) { /* Collect data and put them into the buffer */ } const static tss_task_ops_t *p_tss_task_ops = NULL; typedef struct tss_binary_header { char magic[8]; /* "TSS1.5.0" */ const tss_task_ops_t *(*get_task_ops)(void); } tss_binary_header_t; static int algo_init() { tss_binary_header_t* (*entry)(void); extern uint32_t __base_BINARY_FLASH; entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1); tss_binary_header_t *p_algo_head = entry(); printf("MAGIC NUMBER:"); int i = 0; for(i = 0; i < 8; i++) { printf("%c", p_algo_head->magic[i]); } p_tss_task_ops = p_algo_head->get_task_ops(); if (p_tss_task_ops == NULL) { return -1; } if (p_tss_task_ops->task > TASK_REG || p_tss_task_ops->task < TASK_AD) { return -1; } return 0; } /*! * @brief Main function */ int main(void) { char ch; tss_status status; float probability; assert(algo_init() == 0); const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float)); float *p_targets = (float *)malloc(p_algo_attr->target_num * sizeof(float)); assert(p_data != NULL && p_targets != NULL); status = p_tss_task_ops->reg_ops.init(); if (status != TSS_SUCCESS) { /* Handle the initialization failure cases */ } while (1) { sample_data(p_data); status = p_tss_task_ops->reg_ops.predict(p_data, p_targets); if (status != TSS_SUCCESS) { /* Handle the prediction failure cases */ } /* Handle the prediction result */ } return 0; } ```

> *Notes: The above example is a “Hello World” level code to illustrate the use of the algorithm library or binary for different tasks.* -------------------- ## API Reference > *Notes: The APIs are changed from v1.5 to support both library format and binary format.* ### Files **TimeSeries.h:** The API header file for the library or binary, developers use it for the algorithm integration. ```c #include "TimeSeries.h" ``` ### Enumerations | | name | description | | ------- | ----------- | ---------------------------------------------------------------------- | | typedef | tss_status | Status codes returned from functions in the library or binary | | typedef | task_type_t | Algorithm task type | ```c typedef enum { TSS_SUCCESS = 0, /* No error */ TSS_STATE_ERROR = 1, /* State is incorrect */ TSS_BOARD_ERROR = 2, /* Board information is incorrect */ TSS_MEMORY_ERROR = 3, /* Memory error caused by the HEAP Overflow */ TSS_PREDICT_NOT_ENABLED = 4, /* Predict function is not enabled */ TSS_LEARNING_ERROR = 5, /* Errors occurs during the learning process */ TSS_LEARNING_NOT_ENOUGH = 6, /* Not enough calls to learning */ TSS_RECOMMEND_LEARNING_DONE = 7, /* Reached the recommended calls to learning */ TSS_NOT_READY = 8, /* Function is not ready but planed to support */ TSS_LICENSE_ERROR = 9, /* Invalid license */ TSS_UNKNOWN_ERROR = 10, /* Unknown error */ } tss_status; typedef enum { TASK_AD = 1, TASK_AD_ODL = 2, TASK_CLS = 3, TASK_OC = 4, TASK_REG = 5 } task_type_t; ``` ### Structures | | name | description | | ------- | --------------------- | ---------------------------------------------------------------------- | | typedef | tss_algo_attribute_t | Algorithm attributes | | typedef | tss_ad_task_ops_t | Operations for anomaly detection task | | typedef | tss_ad_odl_task_ops_t | Operations for anomaly detection task with on-device-learning | | typedef | tss_cls_task_ops_t | Operations for n-classification task | | typedef | tss_oc_task_ops_t | Operations for one-class classification task | | typedef | tss_reg_task_ops_t | Operations for regression task | | typedef | tss_task_ops_t | Task-specific operations union | ```c typedef struct { unsigned int data_tab; /* Input data is tabular data, or not */ unsigned int data_len; /* The length of the input data */ unsigned int data_dim; /* The dimension of the input data */ unsigned int model_size; /* The size of the model buffer */ const float *model_addr; /* The address of model buffer that stores the model hyper-parameters */ unsigned int target_num; /* The number fo targets or classes */ float recommend_threshold; /* The recommended threshold */ const char *lib_id; /* Identifier for the library or binary*/ const char *neutron_version; /* The software version of neutron, if supported*/ unsigned int recommend_learning_num; /*The recommended number of learning */ unsigned char odl_supported; /* On-Device-Learning is supported, or not*/ unsigned char neutron_enabled; /* Neutron is enabled, or not */ unsigned char powerquad_enabled; /* PowerQuad is enabled, or not */ } tss_algo_attribute_t; typedef struct tss_ad_task_ops { /** * @brief Initialize the anomaly detection algorithm. * @retval TSS_SUCCESS - Initialization succeed. */ tss_status (*init)(void); /** * @brief Predict the normal probability of the specified data. * @param[in] data_input - The data input for the prediction. * @param[out] probability - The predicted probability output. * @retval TSS_SUCCESS - Prediction succeed. * @retval TSS_PREDICT_NOT_ENABLED - Model not ready for prediction. */ tss_status (*predict)(const float data_input[], float *probability); } tss_ad_task_ops_t; typedef struct tss_ad_odl_task_ops { /** * @brief Initialize the anomaly detection algorithm with the specified model. * @param[in] model_buffer - The model buffer for initialization, NULL means reset the model. * @retval TSS_SUCCESS - Initialization succeed. */ tss_status (*init)(const float model_buffer[]); /** * @brief Learn new model from the normal data. * @param[in] data_input - The data input for the learning. * @retval TSS_SUCCESS - Learning succeed * @retval TSS_LEARNING_NOT_ENOUGH - More data needed for the learning. */ tss_status (*learn)(const float data_input[]); /** * @brief Export the model to the specified buffer. * @param[out] model_buffer - The exported model buffer. * @retval TSS_SUCCESS - Export succeed. * @retval TSS_PREDICT_NOT_ENABLED - Model not ready for export. */ tss_status (*export_model)(float model_buffer[]); /** * @brief Predict the normal probability of the specified data. * @param[in] data_input - The data input for the prediction. * @param[out] probability - The predicted probability output. * @retval TSS_SUCCESS - Prediction succeed. * @retval TSS_PREDICT_NOT_ENABLED - Model not ready for prediction. */ tss_status (*predict)(const float data_input[], float *probability); } tss_ad_odl_task_ops_t; typedef struct tss_cls_task_ops { /** * @brief Initialize the classification algorithm. * @retval TSS_SUCCESS - Initialization succeed. */ tss_status (*init)(void); /** * @brief Predict the probabilities and class index of the specified data. * @param[in] data_input - The data input for the prediction. * @param[out] probabilities - The predicted probabilities of all classes * @param[out] class_index - The predicted class index. * @retval TSS_SUCCESS - Prediction succeed. */ tss_status (*predict)(const float data_input[], float probabilities[], int *class_index); } tss_cls_task_ops_t; typedef struct tss_oc_task_ops { /** * @brief Initialize the one class algorithm. * @retval TSS_SUCCESS - Initialization succeed. */ tss_status (*init)(void); /** * @brief Predict if is outlier and the decision score of the specified data. * @param[in] data_input - The data input for the prediction. * @param[out] is_outlier - The predicted results of if input is outlier. * @param[out] score - The predicted score. * @retval TSS_SUCCESS - Prediction succeed. */ tss_status (*predict)(const float data_input[], float *score, int *is_outlier); } tss_oc_task_ops_t; typedef struct tss_reg_task_ops { /** * @brief Initialize the regression algorithm. * @retval TSS_SUCCESS - Initialization succeed. */ tss_status (*init)(void); /** * @brief Predict the targets based on the specified data. * @param[in] data_input - The data input for the prediction. * @param[out] targets - The predicted targets output. * @retval TSS_SUCCESS - Prediction succeed. */ tss_status (*predict)(const float data_input[], float targets[]); } tss_reg_task_ops_t; typedef struct tss_task_ops { int task; union { tss_ad_task_ops_t ad_ops; tss_ad_odl_task_ops_t ad_odl_ops; tss_cls_task_ops_t cls_ops; tss_oc_task_ops_t oc_ops; tss_reg_task_ops_t reg_ops; }; const tss_algo_attribute_t *(*algo_attribute)(void); } tss_task_ops_t; ``` ### Functions The generated algorithm provides the following main functions: #### tss_get_task_ops() ```c const tss_task_ops_t* tss_get_task_ops(void); ``` **Description:** Returns a pointer to the task operations structure for the generated library. **Returns:** Pointer to `tss_task_ops_t` structure containing task-specific operations and attributes. **Usage:** This is the primary entry point for library format integration. Call this function during initialization and obtain access to all algorithm operations. **Example:** ```c const tss_task_ops_t *p_tss_task_ops = tss_get_task_ops(); if (p_tss_task_ops == NULL) { // Handle error } ``` #### Task-Specific Operations Based on the task type, access the appropriate operations through the returned structure: - **Anomaly Detection:** `p_tss_task_ops->ad_ops` - **Anomaly Detection with ODL:** `p_tss_task_ops->ad_odl_ops` - **Classification:** `p_tss_task_ops->cls_ops` - **One-Class Classification:** `p_tss_task_ops->oc_ops` - **Regression:** `p_tss_task_ops->reg_ops` #### algo_attribute() ```c const tss_algo_attribute_t* (*algo_attribute)(void); ``` **Description:** Retrieves algorithm attributes including data dimensions, model size, and hardware acceleration status. **Returns:** Pointer to `tss_algo_attribute_t` structure. **Example:** ```c const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute(); printf("Data length: %u, Data dimension: %u\n", p_algo_attr->data_len, p_algo_attr->data_dim); ``` ## Algorithm Project Execution eIQ Time Series Studio helps generate the sample project, which can be directly imported in the MCUXpresso IDE. The sample project contains a generated algorithm library or binary, time series framework, your target project driver, settings, and components. You can take the sample project as a **QuickStart** with your own library or binary. Sample project workflow overview: ![alt text](_static/picture/deployment/sample_prj_wkflow.jpg) - Idle state. Ready to handle the SHELL commands and collect the sensor data by the sensor HAL in time series framework. - Data log state. Print the sensor data via SHELL over UART. - Prediction state. Predict based on the sensor data by the generated model algorithm and print the results via SHELL over UART. - On-device-Learn state. Learn a new model from the sensor data by the generated model algorithm and print the results via SHELL over UART. Sample Projects key features: - **QuickStart** with your algorithm on the target Edge device. - User-friendly **SHELL** in the serial terminal, start the learning/prediction process with commands. - Provides an option to **log** the data when the target has an embedded sensor (accelerator). - To test the algorithm without a physical sensor as the data input, use **a dummy sensor HAL** in the Time Series framework. Based on the MCX-N9XX-EVK, the file tree of the **generated sample project** is shown as below. 📦MCX-N9XX-EVK Choose the build option for project with library or binary. ┣ 📂Framework time series framework based on the FreeRTOS. ┃ ┣ 📂core ┃ ┣ 📂docs ┃ ┣ 📂hal Hardware Abstraction Layer. ┃ ┃ ┣ 📂inc ┃ ┣ 📂inc ┗ 📂MCX-N9XX-EVK Base Project. ┃ ┣ 📂CMSIS ┃ ┣ 📂board ┃ ┣ 📂component ┃ ┣ 📂device ┃ ┣ 📂drivers ┃ ┣ 📂freertos ┃ ┣ 📂source ┃ ┃ ┣ 📂TimeSeries Generated time series library or binary. ┃ ┃ ┣ 📜FreeRTOSConfig.h FreeRTOS config header file. ┃ ┃ ┣ 📜cpp_config.cpp ┃ ┃ ┣ 📜hardware.c Config file of the hardware/sensors. ┃ ┃ ┣ 📜lptmr.c ┃ ┃ ┣ 📜lptmr.h ┃ ┃ ┣ 📜main.c Main program. ┃ ┃ ┣ 📜memory.c ┃ ┃ ┗ 📜semihost_hardfault.c ┃ ┣ 📂startup ┃ ┣ 📂usb ┃ ┣ 📂utilities ┃ ┣ 📜.cproject ┃ ┣ 📜.gitignore ┃ ┣ 📜.project ┃ ┗ 📜README.pdf User Guide of the sample project. ### SHELL Interface After clicking **GENERATE** with the project option and completing the build-flash steps, the time series sample project flashes directly into your device. Open the **Serial Terminal** and start the **execution**: ![alt text](_static/picture/deployment/dep_shell_demo.gif) The **command-line interface** is straightforward as reflected in the output from ```help```: ```c "help": List all the registered commands "exit": Exit program "start : Start an execution - log: Start data logger - learn: Start time series learning - reset: Start time series knowledge reset - pre: Start time series prediction "stop": Stop ongoing execution "setup : Setup a parameter - odr: Setup output data rate - fsr: Setup full scale range - sc: Setup sample count - thold: Setup prediction threshold (Anomaly Detection Only) "loadlib : dynamic load a library to allocated memory - alloc size: allocate memory of size bytes - load line: load one line of library to memory "get : Get board information - info: Get system information - state: Get current Time Series state - range: Get parameter range ``` ### Button interface To execute the “start pre”, “start learn”, and “stop” of shell instructions, the sample project supports a simple **button interface 🔘** on the board. - If there is a support for two buttons on the board, toggling them means toggling “start pre/stop”, and “start learn/stop”. - If there is support for only one button, toggling means “start pre/stop”. - If the prediction or learn or data log is ongoing, press any supported button stops the execution. **🏆 Congratulations!** *You have completed the whole process from the data import to the final algorithm library or binary generation. You can now proceed with the time series AI/ML algorithm deployment for your real device.*