# Quick Start
This section lists the steps from data input to algorithm generation. To demonstrate the sample application from the homepage of the IDE, perform the following steps. Several sample applications are included and updated when new samples become available.
**BYOD workflow diagram:**
**BYOM workflow diagram:**
The following is a summary of steps based on the above diagrams.
**1) Task Selection**
- Select the appropriate task (Anomaly Detection, n-Class Classification, 1-Class Classification, or Regression) based on your use case.
**2) Project Creation**
- Select `AutoML Project` or `BYOM Project`.
- Provide a name for your project with essential descriptions.
- Select the target board on which you want to deploy the final algorithm. Alternatively, select a CPU-compatible board if your specific board does not exist.
- Specify the RAM and flash size limits or keep all as '0' if you do not want any limitations for model training.
- Input the proper values for channel number, class number, and target according to your task selection.
**3) Dataset Loading**
- If your project is BYOM, then dataset loading is used for model quantization and is optional if you do not want model quantization.
- It is mandatory to prepare the dataset before training. For demonstration, you can collect your own data or use some public datasets.
- You can visualize the dataset in raw format, temporal, statistical, and spectral domains with different operators.
**4) Model Training**
- Model training is the core technology that runs auto machine learning for automatic hyperparameter searching and optimization.
- Supports both classical machine learning and deep learning models with the best-fit algorithm pipeline selected automatically.
- Auto-optimization to get the best model list based on accuracy, flash, and RAM size as weights for ranking scores.
- Shows the training progress for accuracy, flash, RAM, and the metric details for each candidate model.
**5) Model Input**
- Model input is only for BYOM to allow importing third-party models for conversion and quantization.
- Shows the model benchmark results for both FP32 and INT8 with R2 and MSE metrics.
- Shows the model network structure with all layers parsed if the conversion is successful.
**6) Model Emulation**
- Lists all the candidate models for each training session and supports batch selection for automatic emulation testing.
- Emulation can help check if the trained model overfits or if the accuracy meets expectations.
- Easily manage the emulation report with all model details.
**7) Model Deployment**
- Supports automatic code or library compilation and generation for the specified CPU core and IDE.
- Generates the core algorithm library and the API header file. If the board is in the support list, it generates a MCUXpresso sample package.
- Provides sample application code as a quick reference.
## Launch eIQ Time Series Studio
When the eIQ Time Series Studio application launches, a workspace selection dialog appears as shown below. Select a workspace directory where your projects and data are stored.
After the workspace selection completes, the application launches, Loading may take some time, depending on your PC configuration and network conditions.
During the launch, the cloud server checks your eIQ Time Series Studio version. If your IDE version is outdated, a dialog box appears and recommends that you upgrade to the latest version.
**You have two options:**
- If you use an old version, there is a risk that some functions are restricted or some known bugs still exist.
- To avoid any restrictions, choose to accept and upgrade your IDE to the latest version.
## Telemetry Consent Acceptance
eIQ Time Series Studio requires user consent for telemetry data collection to help improve product features and user experience.
You have two options for telemetry consent:
- To reject the telemetry data collection and exit using the eIQ Time Series Studio, click `Opt Out and Disable Tool`.
- To accept telemetry data collection and continue using the eIQ Time Series Studio, click `OK and Proceed`.
## Login NXP Account
eIQ Time Series Studio requires user login with an NXP account to allow unlimited algorithm library generation. Your login status remains active until you log out. Therefore, you do not need to log in again the next time you launch eIQ Time Series Studio.
### NXP Employee Login
- Click `Employee Sign In` for NXP internal users through the NXP SSO login process.
- Follow the next account selection steps and easily complete the NXP employee login process.
### External User Login
**The standard NXP account login process required by NXP websites.**
- Click `CREATE AN ACCOUNT` if you are a new user and have never had an NXP user account. Follow the standard steps and complete the new user registration.
- Once you have an NXP user account, input your `Email Address` and `Password`, then click `SIGN IN` to complete the login process.
- After successful login, you can use all the functions. The top-right corner shows your login status.
**Tips:**
To log out of the IDE, click the `Logout` icon. However, you must log in again to continue using the IDE.
## Function Panel
Here is a brief description of the main functions.
**Home**
- Contains sample applications with sample datasets and a quick guide for anomaly detection, n-class classification, 1-class classification, and regression tasks.
**Tasks**
- **Anomaly Detection**
Sample applications for anomaly detection from project creation to algorithm library generation.
- **n-Class Classification**
Sample applications for multiclass classification from project creation to algorithm library generation.
- **1-Class Classification**
Sample applications for single-class classification from project creation to algorithm library generation.
- **Regression**
Sample applications for regression from project creation to algorithm library generation.
**Utilities**
- **Data Logging**
Supports external user boards to capture sensor datasets through the COM port and save them for training.
- **Data Labeling**
Supports labeling raw continuous data into different sections of labeled data.
- **Data Operations**
Supports converting labeled continuous data to segmented data for training and emulation.
- **Data Intelligence**
Supports smart analysis of dataset quality.
Supports smart analysis of continuous datasets to find the best sample rate and window size.
Converts continuous data to segmented data and automatically saves it for training.
**Solutions**
- **AFCI**
Solutions for "Arc Fault Circuit Interrupter" workflow to build from dataset to AFCI algorithm.
**Support**
- **Documentation**
An online user guide with technical details updated on the cloud server.
- **About**
Provides the IDE version ID.
**Tips:**
For better space layout, click the button highlighted below and you can hide and show the function panel.
## Task Selection
Task selection is the first step to select the algorithm. You can select **Anomaly Detection**, **n-Class Classification**, **1-Class Classification**, or **Regression**. After selecting the task, follow the wizard to complete the steps of `Projects`, `Dataset`, `Training`, `Emulation`, and `Deployment`.
## Project Creation
Click the `Projects` tab and then click the `Create New Project` button and complete the project settings for the task. Different tasks have different input items. For details, see the `CREATE PROJECT` section.
## Dataset Loading
Click the `Dataset` tab and load your training data files for the task. Different tasks have different input items. Data visualization supports raw format, temporal, statistical, and spectral domains. For details, see the `INPUT DATA` section.
## Model Training
Click the `Training` tab after the dataset loads. The training function is the core technology that contains automation for algorithm hyperparameter searching, benchmarking, and optimization for the best accuracy while fitting within restricted flash and RAM sizes. For details, see the `START TRAINING` section.
## Model Input
Click the `Model Input` tab if the project was created for BYOM. Then click the `Start New Conversion` button, and a pop-up window appears to configure the conversion name, model selection, and quantization type. For details, see the `Bring Your Own Model` section.
## Model Emulation
Click the `Emulation` tab after training completes or when partial training results are already obtained. The emulation function is an important and innovative feature that helps:
- Verify/test real data and check if the algorithm overfits or if the accuracy meets expectations.
- Select all the models listed to benchmark all metrics.
- Find bugs in the deployment library.
Emulation requires public network support as the emulation executable image is dynamically generated from the cloud server. For details, see the `EMULATION & BENCHMARK` section.
## Model Deployment
Click the `Deployment` tab after emulation is completed and you have selected the best model. The deployment function gets the optimized algorithm library and deploys it to real hardware.
Deployment requires public network support as the target library for a specific CPU and the target model. The target IDE requirement is dynamically generated from the cloud server. For details, see the `DEPLOYMENT` section.