TF Lite Quantizer¶
This tool quantizes a FLOAT (FP16/FP32) TensorFlow Lite model using profiling guided quantization. The quantizer uses dynamic range information from a profile file (generated by tflite-profiler) to determine optimal quantization parameters for each tensor.
Prerequisites¶
Model must be a FLOAT TensorFlow Lite model.
Profile file must be generated using tflite-profiler with the same model and representative dataset.
Usage¶
The tflite-quantizer has the following syntax:
tflite-quantizer --input <input_model_path> --profile <profile_file_path> [OPTIONS]
Required Parameters¶
--input- The path to the input FLOAT TensorFlow Lite model.--profile- The path to the input profile file in CSV format generated by tflite-profiler. The profile file contains dynamic range information with the following structure:<tensor1_index>,<tensor1_min>,<tensor1_max>,<tensor1_histogram_bin1>,<tensor1_histogram_bin2>,..,<tensor1_histogram_binN>, <tensor2_index>,<tensor2_min>,<tensor2_max>,<tensor2_histogram_bin1>,<tensor2_histogram_bin2>,...<tensor2_histogram_binN>, ...
Optional Parameters¶
--output- The path for the output quantized TensorFlow Lite model. If not provided, the output model will be written in the same directory as the input model with the suffix _quantized added to the filename.--graph-name- For models with multiple graphs, this specifies the name of the graph to quantize. This parameter is ignored for single-graph models.
Quantization Configuration Parameters¶
Global Quantization Options¶
--quantize-inputs- Whether to quantize the input graph placeholders. Options:True,False. Default isTrue.--quantize-outputs- Whether to quantize the output graph placeholders. Options:True,False. Default isTrue.--quantize-constants- Whether to quantize the constant tensors (weights). Options:True,False. Default isTrue.--quantize-variables- Whether to quantize the variable tensors (activations). Options:True,False. Default isTrue.
Data Type Configuration¶
--quantization-constant-type- The data type for quantizing constant tensors (weights). Options:INT8,INT16,INT32. Default isINT8.--quantization-constant-type-bias- The data type for quantizing bias tensors in Conv2D, DepthwiseConv2D, TransposeConv2D, Conv3D, TransposeConv3D, and FullyConnected operations. Options:INT8,INT16,INT32. Default isINT32.--quantization-variable-type- The data type for quantizing variable tensors (activations). Options:INT8,INT16,INT32. Default isINT8.
Granularity and Schema Configuration¶
--quantization-constant-granularity- The granularity for quantizing constant weight tensors in Conv2D, DepthwiseConv2D, TransposeConv2D, Conv3D, and TransposeConv3D operations. Options:PTQ(Per-Tensor Quantization),PCQ(Per-Channel Quantization). Default isPCQ.--quantization-constant-schema- The schema for quantizing constant tensors (weights). Options:Asymmetric,Symmetric,SymmetricWithPower2Scale. Default isSymmetric.--quantization-variable-schema- The schema for quantizing variable tensors (activations). Options:Asymmetric,Symmetric,SymmetricWithPower2Scale. Default isAsymmetric.
Custom Quantization Options¶
--quantization-variable-custom-symmetric- Option to enable special quantization for Mul and BatchMathMul variable inputs. Default isfalse.
Profiling configuration¶
--quantization-calibration-method- Method used to determine quantization range for each tensor. Options:MinMax(takes Min/Max values from profiling),Percentile(remove outliers according to the value specified in--quantization_percentile_val). Default isMinMax.--quantization-percentile-val- Percentile-based clipping value. Preserve the central portion of the histogram symmetrically. Default is99.9.
Operator-Level Control¶
Operator Type Filtering¶
--quantize-operator-types-except- Exclude specific operator types from quantization. Accepts comma-separated list of operator names or indices (e.g.,ADD,AVERAGE_POOL_2Dor0,1).--quantize-operator-types-only- Only quantize specific operator types. Accepts comma-separated list of operator names or indices (e.g.,ADD,AVERAGE_POOL_2Dor0,1).
Beside individual operators, there is also the option to exclude from quantization various macro operators sensitive to quantization, such as Layer Norm. If layernorm is specified in the --quantize-operator-types-except flag, the lowered pattern of Layer Norm is identified and completely excluded from quantization.
Note:
The
exceptandonlyoptions can be combined for both operator types and instances.Operator identification: Use operator index or the name of the first output tensor (operators don’t have standalone names)
Debugging and Validation Options¶
--run-after-quantize- Validates the quantized model by running it with the TFLite interpreter using dummy input data. This option only works with standard quantization configurations supported by TFLite interpreter (e.g., INT8 with default parameters). Options:True,False. Default isFalse.--verbose- Enables detailed console output including quantization constraints applied to the graph. Options:True,False. Default isFalse.
Example¶
tflite-quantizer --input model.tflite --profile model_profile.csv --output model_quantized.tflite --verbose True
This command quantizes model.tflite using the profile information from model_profile.csv, saves the result as model_quantized.tflite, and enables verbose output for debugging.