MCUXpresso SDK Compatibility Matrix

Ensure to keep Neutron Driver, Firmware and Converter in sync (from the same Neutron SDK).
Not having the runtime binaries and converted model aligned can result in unreliable operation.
A microcode version mismatch message is printed to warn the user if runtime binaries and converted model are not aligned.

Microcode version mismatch! Model converted with 3.0.0-0X7dbce418

The following table shows the compatibility between MCUXpresso SDK versions and Neutron SDK versions:

Neutron SDK Version

Found in release

MCU SDK
25.03

MCU SDK
25.06

MCU SDK
25.09

MCU SDK
25.12

MCU SDK
26.03

MCU SDK
26.06

1.2.0

eIQ Toolkit 1.15 (Windows, Ubuntu 20.04)

Default

2.0.2

eIQ Toolkit 1.16 (Windows, Ubuntu 20.04)

Upgradable

Default

2.1.3

eIQ Toolkit 1.17 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Default

2.2.2

eIQ Neutron SDK 2.2.2 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Default

2.2.3

eIQ Neutron SDK 2.2.3 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Upgradable

Upgradable

3.0.0

eIQ Neutron SDK 3.0.0 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Upgradable

Default

Upgradable

3.0.1

eIQ Neutron SDK 3.0.1 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Upgradable

Upgradable

3.1.0

eIQ Neutron SDK 3.1.0 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Upgradable

Upgradable

3.1.1

eIQ Neutron SDK 3.1.1 (Windows, Ubuntu 20.04)

Upgradable

Upgradable

Upgradable

Upgradable

Default

 

Note

  • Default - MCUXpresso SDK includes runtime components (driver, firmware) corresponding to Neutron SDK version.

    • Example: Neutron SDK version 3.0.0 runtime binaries included in MCUXpresso SDK 26.03.

  • Upgradable - requires upgrading runtime components (driver, firmware) and performing model conversion with corresponding Neutron Converter.

    • Example: Neutron SDK version 3.1.0 runtime binaries can be used with MCUXpresso SDK 26.03 if runtime components upgrade is performed and model converted with Neutron Converter 3.1.0