Deployment

❗Important: The library/binary generated by eIQ Time Series Studio is licensed exclusively for use on NXP devices. It must be implemented and deployed solely on NXP products.

After completing Emulation and identifying the optimal model, switch to the “Deployment” tab to generate and deploy the optimized algorithm. The Deployment process generates the optimized algorithm library or binary along with a sample project, which can then be offloaded to edge devices.

The Deployment section represents the final stage of the pipeline. It provides step-by-step guidance to generate and deploy the algorithm for your project on target devices.

Notes: Deployment requires public network support because the Cloud Server dynamically generates target libraries or binaries specific to your CPU, model, and IDE.


Function Layout

alt text

The Deployment section of eIQ Time Series Studio supports the following main functions:

Supported Algorithm Formats

The final deliverable of the algorithm supports two optional formats:

  • *Library(*.a or .lib): Updating the algorithm requires relinking and rebuilding the entire firmware project.

  • Binary(*.bin): The algorithm can be updated independently by updating only the corresponding firmware section, without requiring a full firmware upgrade.

Notes: Currently, the binary format is supported only on the FRDM‑MCXN947 target. Support for more targets will be added in future releases.

Supported Compilers

eIQ Time Series Studio supports the following compilers:

  • GCC (MCUXpresso, GNU ARM Embedded Toolchain)

  • Arm Compiler (Keil MDK)

  • IAR Compiler (IAR Embedded Workbench For Arm)

alt text

  • CodeWarrior (CodeWarrior Development Studio For DSC)

alt text

Supported Architectures

  • Arm Cortex-M series (widely used in microcontrollers)

  • NXP DSC cores (Digital Signal Controllers)

  • Arm Cortex-A series (via GCC)

Supported Compilation Flags

The supported compilation flags are:

  • float-abi: Specifies which floating-point ABI to use. (hard/soft). Default: hard.

  • fshort-wchar: Sets the size of wchar_t. Default: -fno-short-wchar.

  • fshort-enums: Sets the enumeration type to the smallest data type that can hold all enumerator values. Default: -fshort-enums for GCC, -fno-short-enums for Arm Compiler.

Notes: Reference from the Arm Compiler Reference Guide.

Supported Accelerator Options

  • PowerQuad DSP: Accelerates FFT calculation. The target device must contain this hardware.

  • Neutron NPU: Accelerates deep learning model predictions. The target device must contain this hardware.

Multi-Library Generation

Multi-Library enables users to link multiple TSS libraries within the same project or device, allowing each library to operate independently. In industrial and home appliance applications, projects often integrate multiple sensor types and models that simultaneously provide independent time series data at different sampling rates.

The Multi-Library feature enables users to deploy dedicated TSS libraries for each independent set of time series data. Each library can incorporate different algorithm types, such as Anomaly Detection, Classification, or Regression. The inference results can be processed independently or combined to support higher-level, systemwide decision-making.

alt text

Libraries are differentiated by customized suffix names in the Deployment section. The suffix is applied consistently to the library filename, header filename, macro definitions, and API symbols in the header file. By invoking APIs with distinct suffix names, the application can explicitly select the corresponding TSS library, enabling multiple libraries to coexist within the same project without naming conflicts.

Notes: The generation of sample projects is not supported when the Multi-Library generation is enabled.


Deployment Process

Library Format Deployment Steps

alt text

Follow the steps and generate your own time series library and deploy it to your devices:

  1. Select Format: Choose Library as the algorithm format type.

  2. Select Model: Pick the best quality model from the Emulation process.

  3. Select CPU Core: Choose the CPU core of the target board.

  4. Project Generation: Decide whether to generate with a MCUXpresso project.

  5. Suffix Name: Set library suffix for Multi-Library projects (optional).

  6. Compiler: Choose a compiler (“CodeWarrior” for DSC core).

  7. Accelerator Options: Configure the hardware accelerator if supported.

  8. Compilation Flags: Select optimal flags for the compiler.

  9. Generate: Click GENERATE button and create library or project from Cloud.

  10. Download: Download and unzip the generated package.

  11. Deploy: Link the library to your project or import the generated project to MCUXpresso IDE, build the project, and flash to the target device.

Binary Format Deployment Steps

alt text

Follow the steps and generate your own time series binary and deploy it to your devices:

  1. Select Format: Choose Binary as the algorithm format type.

  2. Configure Section: Set binary configuration parameters for deployment. Ensure that the configuration matches to the firmware project settings.

alt text

  1. Select Model: Pick the best quality model from the Emulation process.

  2. Select CPU Core: Choose the CPU core of the target board.

  3. Project Generation: Decide whether to generate with a MCUXpresso project.

  4. Compiler: Choose the compiler. Currently, only “GCC” is supported for binary format.

  5. Accelerator Options: Configure the hardware accelerator if supported.

  6. Compilation Flags: Select optimal flags for the compiler.

  7. Generate: Click GENERATE button and create binary or project from Cloud.

  8. Download: Download and unzip the generated package.

  9. Deploy: Flash the binary to the target device in the designated algorithm firmware section. Import the generated project to MCUXpresso IDE to know how to use the binary in your application.

LinkServer(inc. CMSIS-DAP) Programming Support

Programming via LinkServer(inc. CMSIS-DAP) is supported. Ensure that the target board is connected to your PC through a LinkServer debugger before proceeding.

  1. Refresh to list the connected LinkServer probe.

  2. Select the desired LinkServer probe from the list.

  3. Click PROGRAM and flash the binary to the target device in the designated algorithm firmware section.


Algorithm Integration

eIQ Time Series Studio Library/Binary is an algorithm library or binary for edge devices. The time series cloud server dynamically generates embedded C/C++ code and cross-compiles based on your specific hardware and compiler information.

alt text

Generated Package Structure

Library Package:

    📦_libtss
    ┣ 📜algorithm.dat
    ┣ 📜libtss.a or tss.lib
    ┣ 📜LICENSE.txt
    ┣ 📜metadata.json
    ┗ 📜TimeSeries.h

Binary Package:

    📦_binary
    ┣ 📜algorithm.dat
    ┣ 📜libtss.bin
    ┣ 📜LICENSE.txt
    ┣ 📜metadata.json
    ┗ 📜TimeSeries.h
  • algorithm.dat: The encrypted file with the algorithm details. NXP cloud server can parse and generate the source code.

  • libtss.a / tss.lib / libtss.bin: The core algorithm library or binary; developers use it for algorithm integration. (If Arm Compiler or CodeWarrior is selected, the generated library is tss.lib)

  • LICENSE.txt: NXP online code hosting software license agreement.

  • metadata.json: The meta description file for the generated algorithm. The file contains key information like compiler type, task type, input dataset, and platform information. The file also contains the minimum memory size as reference.

  • TimeSeries.h: The API header file for the library or binary, developers use it for the algorithm integration.

Sample Code Integration

The documentation provides sample code examples for integrating the library or binary into your project for different task types (Anomaly detection, n-Class Classification, 1-Class Classification, Regression, and Forecasting).

Sample Code For Library

Anomaly detection
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

static int algo_init()
{
    p_tss_task_ops = tss_get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    float probability;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    assert(p_data != NULL);

    if (p_tss_task_ops->task == TASK_AD_ODL)
    {
        /*
         * It's also ok that input pre-learned knowledge stored in p_algo_attr->model_addr.
         * Here we use online learning to train the model with normal data samples.
         * Input NULL to skip pre-learned knowledge.
         */
        status = p_tss_task_ops->ad_odl_ops.init(NULL);
        if (status != TSS_SUCCESS)
        {
            /* Handle the initialization failure cases */
        }
        /*The learning number is customizable, but we recommend the number greater than TSS_RECOMMEND_LEARNING_SAMPLE_NUM to get better results.*/
        int learning_num = p_algo_attr->recommend_learning_num;
        for (int i = 0; i < learning_num; i++)
        {
            sample_data(p_data);
            status = p_tss_task_ops->ad_odl_ops.learn(p_data);
            if (status != TSS_LEARNING_NOT_ENOUGH && status != TSS_RECOMMEND_LEARNING_DONE)
            {
                /* Handle the learning failure cases */
            }
        }
    }
    else
    {
        status = p_tss_task_ops->ad_ops.init();
    }

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        if (p_tss_task_ops->task == TASK_AD_ODL)
        {
            status = p_tss_task_ops->ad_odl_ops.predict(p_data, &probability);
        }
        else
        {
            status = p_tss_task_ops->ad_ops.predict(p_data, &probability);
        }
        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
n-Class Classification
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

static int algo_init()
{
    p_tss_task_ops = tss_get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    int class_index;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    float *p_result = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_result != NULL);

    status = p_tss_task_ops->cls_ops.init();


    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->cls_ops.predict(p_data, p_result, &class_index);

        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
1-Class Classification
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

 /* Decision score indicating anomaly/outlier status. Positive values (score > 0) indicate normal samples,
 * while negative values suggest outliers/anomalies. is_outlier flag is derived by thresholding at 0.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

static int algo_init()
{
    p_tss_task_ops = tss_get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    int is_outlier;
    float score;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    assert(p_data != NULL);

    status = p_tss_task_ops->oc_ops.init();


    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->oc_ops.predict(p_data, &score, &is_outlier);

        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
Regression
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

static int algo_init()
{
    p_tss_task_ops = tss_get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    float *p_targets = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_targets != NULL);

    status = p_tss_task_ops->reg_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->reg_ops.predict(p_data, p_targets);
        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
Forecasting
/*
 * Copyright 2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect sample data. 
        - If data for all channels is available (non-recursive), put them into the buffer and return 0. 
        - If data for part of channels is available (recursive with covariate channels), put them into the buffer and return -1 
        - If no data for any channel is available (recursive without covariate channels), return -2 
    */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

static int algo_init()
{
    p_tss_task_ops = tss_get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    /* Remark:p_algo_attr->target_num = forecast horizons num x forecast channels num 
               horizon num = 1 for recursive forecast */
    float *p_forecasts = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_forecasts != NULL);

    status = p_tss_task_ops->fc_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }

    uint32_t recursive_cnt = 0;
    uint32_t sample_data_len = p_algo_attr->data_dim * p_algo_attr->data_len;
    while(1) 
    {
        int data_status = sample_data(p_data);

        if (p_algo_attr->recursive_predicted == false)/* Non-recursive forecasting case */
        {
            if (data_status < 0)
            {
                /* Handle the failure case and exit the prediction*/
            }
            else
            {
                status = p_tss_task_ops->fc_ops.predict(p_data, p_forecasts);
                if (status != TSS_SUCCESS)
                {
                    /* Handle the prediction failure cases */
                }
                /* Handle the forecasting result */
            }
        }
        else /* recursive forecasting case */
        {                 
            if (recursive_cnt)
            {
                /* If the first recursive forecast has completed, 
                   use the previously forecasted values as the lastest sample for the corresponding channels
                   in the next recursive forecasting iteration. 
                */       
                for (int i = 0; i < p_algo_attr->target_num; i++)
                {
                    uint32_t forecast_channel_idx = p_algo_attr->forecast_channels[i] - 1;
                    p_data[sample_data_len - p_algo_attr->data_dim + forecast_channel_idx] = p_forecasts[i];
                }
            }

            status = p_tss_task_ops->fc_ops.predict(p_data, p_forecasts);
            if (status != TSS_SUCCESS)
            {
                /* Handle the prediction failure cases */
            }

            recursive_cnt++;  
                
            /* Move the data window forward by one time step for the next recursive prediction */
            memmove(p_data, p_data + p_algo_attr->data_dim, sizeof(float)*(sample_data_len - p_algo_attr->data_dim));
            
            if (recursive_cnt == p_algo_attr->recursive_length)
            {/* Remark: The condition to end recursive forecasting can be customized */ 
                /* Handle the recursive forecasting ending case */
            }

            /* Handle the forecasting result */
        }
    }
    return 0;
}

Sample Code For Binary

Anomaly detection
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

typedef struct tss_binary_header
{
    char magic[8];
    const tss_task_ops_t *(*get_task_ops)(void);
} tss_binary_header_t;

static int algo_init()
{
    tss_binary_header_t* (*entry)(void);
    extern uint32_t __base_BINARY_FLASH;
    entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1);
    tss_binary_header_t *p_algo_head = entry();
    printf("MAGIC NUMBER:");
    int i = 0;
    for(i = 0; i < 8; i++)
    {
        printf("%c", p_algo_head->magic[i]);
    }
    p_tss_task_ops = p_algo_head->get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    float probability;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    assert(p_data != NULL);

    if (p_tss_task_ops->task == TASK_AD_ODL)
    {
        /*
         * It's also ok that input pre-learned knowledge stored in p_algo_attr->model_addr.
         * Here we use online learning to train the model with normal data samples.
         * Input NULL to skip pre-learned knowledge.
         */
        status = p_tss_task_ops->ad_odl_ops.init(NULL);
        if (status != TSS_SUCCESS)
        {
            /* Handle the initialization failure cases */
        }
        /*The learning number is customizable, but we recommend the number greater than TSS_RECOMMEND_LEARNING_SAMPLE_NUM to get better results.*/
        int learning_num = p_algo_attr->recommend_learning_num;
        for (int i = 0; i < learning_num; i++)
        {
            sample_data(p_data);
            status = p_tss_task_ops->ad_odl_ops.learn(p_data);
            if (status != TSS_LEARNING_NOT_ENOUGH && status != TSS_RECOMMEND_LEARNING_DONE)
            {
                /* Handle the learning failure cases */
            }
        }
    }
    else
    {
        status = p_tss_task_ops->ad_ops.init();
    }

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        if (p_tss_task_ops->task == TASK_AD_ODL)
        {
            status = p_tss_task_ops->ad_odl_ops.predict(p_data, &probability);
        }
        else
        {
            status = p_tss_task_ops->ad_ops.predict(p_data, &probability);
        }
        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
n-Class Classification
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

typedef struct tss_binary_header
{
    char magic[8];
    const tss_task_ops_t *(*get_task_ops)(void);
} tss_binary_header_t;

static int algo_init()
{
    tss_binary_header_t* (*entry)(void);
    extern uint32_t __base_BINARY_FLASH;
    entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1);
    tss_binary_header_t *p_algo_head = entry();
    printf("MAGIC NUMBER:");
    int i = 0;
    for(i = 0; i < 8; i++)
    {
        printf("%c", p_algo_head->magic[i]);
    }
    p_tss_task_ops = p_algo_head->get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    int class_index;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    float *p_result = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_result != NULL);

    status = p_tss_task_ops->cls_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->cls_ops.predict(p_data, p_result, &class_index);
        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
1-Class Classification
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

 /* Decision score indicating anomaly/outlier status. Positive values (score > 0) indicate normal samples,
 * while negative values suggest outliers/anomalies. is_outlier flag is derived by thresholding at 0.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

typedef struct tss_binary_header
{
    char magic[8];
    const tss_task_ops_t *(*get_task_ops)(void);
} tss_binary_header_t;

static int algo_init()
{
    tss_binary_header_t* (*entry)(void);
    extern uint32_t __base_BINARY_FLASH;
    entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1);
    tss_binary_header_t *p_algo_head = entry();
    printf("MAGIC NUMBER:");
    int i = 0;
    for(i = 0; i < 8; i++)
    {
        printf("%c", p_algo_head->magic[i]);
    }
    p_tss_task_ops = p_algo_head->get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;
    int is_outlier;
    float score;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    assert(p_data != NULL);

    status = p_tss_task_ops->oc_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->oc_ops.predict(p_data, &score, &is_outlier);
        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
Regression
/*
 * Copyright 2024-2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect data and put them into the buffer */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

typedef struct tss_binary_header
{
    char magic[8];
    const tss_task_ops_t *(*get_task_ops)(void);
} tss_binary_header_t;

static int algo_init()
{
    tss_binary_header_t* (*entry)(void);
    extern uint32_t __base_BINARY_FLASH;
    entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1);
    tss_binary_header_t *p_algo_head = entry();
    printf("MAGIC NUMBER:");
    int i = 0;
    for(i = 0; i < 8; i++)
    {
        printf("%c", p_algo_head->magic[i]);
    }
    p_tss_task_ops = p_algo_head->get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    char ch;
    tss_status status;
    float probability;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    float *p_targets = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_targets != NULL);

    status = p_tss_task_ops->reg_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }
    while (1)
    {
        sample_data(p_data);
        status = p_tss_task_ops->reg_ops.predict(p_data, p_targets);

        if (status != TSS_SUCCESS)
        {
            /* Handle the prediction failure cases */
        }
        /* Handle the prediction result */
    }
    return 0;
}
Forecasting
/*
 * Copyright 2026 NXP
 * NXP Confidential and Proprietary. This software is owned or controlled by NXP and may only be used
 * strictly in accordance with the applicable license terms. By expressly accepting such terms or by
 * downloading, installing, activating and/or otherwise using the software, you are agreeing that you
 * have read, and that you agree to comply with and are bound by, such license terms. If you do not
 * agree to be bound by the applicable license terms, then you may not retain, install, activate or
 * otherwise use the software.
 */

#include <stdlib.h>
#include <assert.h>
#include <stdio.h>
#include <stdint.h>
#include "TimeSeries.h"

static void sample_data(float data_buffer[])
{
    /* Collect sample data. 
        - If data for all channels is available (non-recursive), put them into the buffer and return 0. 
        - If data for part of channels is available (recursive with covariate channels), put them into the buffer and return -1 
        - If no data for any channel is available (recursive without covariate channels), return -2 
    */
}

const static tss_task_ops_t *p_tss_task_ops = NULL;

typedef struct tss_binary_header
{
    char magic[8];
    const tss_task_ops_t *(*get_task_ops)(void);
} tss_binary_header_t;

static int algo_init()
{
    tss_binary_header_t* (*entry)(void);
    extern uint32_t __base_BINARY_FLASH;
    entry = (tss_binary_header_t* (*)(void))(uintptr_t)(&__base_BINARY_FLASH + 1);
    tss_binary_header_t *p_algo_head = entry();
    printf("MAGIC NUMBER:");
    int i = 0;
    for(i = 0; i < 8; i++)
    {
        printf("%c", p_algo_head->magic[i]);
    }
    p_tss_task_ops = p_algo_head->get_task_ops();

    if (p_tss_task_ops == NULL)
    {
        return -1;
    }
    if (p_tss_task_ops->task > TASK_FC || p_tss_task_ops->task < TASK_AD)
    {
        return -1;
    }
    return 0;
}

/*!
 * @brief Main function
 */
int main(void)
{
    tss_status status;

    assert(algo_init() == 0);

    const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
    float *p_data = (float *)malloc(p_algo_attr->data_len * p_algo_attr->data_dim * sizeof(float));
    /* Remark:p_algo_attr->target_num = forecast horizons num x forecast channels num 
               horizon num = 1 for recursive forecast */
    float *p_forecasts = (float *)malloc(p_algo_attr->target_num * sizeof(float));
    assert(p_data != NULL && p_forecasts != NULL);

    status = p_tss_task_ops->fc_ops.init();

    if (status != TSS_SUCCESS)
    {
        /* Handle the initialization failure cases */
    }

    uint32_t recursive_cnt = 0;
    uint32_t sample_data_len = p_algo_attr->data_dim * p_algo_attr->data_len;
    while(1) 
    {
        int data_status = sample_data(p_data);

        if (p_algo_attr->recursive_predicted == false)/* Non-recursive forecasting case */
        {
            if (data_status < 0)
            {
                /* Handle the failure case and exit the prediction*/
            }
            else
            {
                status = p_tss_task_ops->fc_ops.predict(p_data, p_forecasts);
                if (status != TSS_SUCCESS)
                {
                    /* Handle the prediction failure cases */
                }
                /* Handle the forecasting result */
            }
        }
        else /* recursive forecasting case */
        {                 
            if (recursive_cnt)
            {
                /* If the first recursive forecast has completed, 
                   use the previously forecasted values as the lastest sample for the corresponding channels
                   in the next recursive forecasting iteration. 
                */       
                for (int i = 0; i < p_algo_attr->target_num; i++)
                {
                    uint32_t forecast_channel_idx = p_algo_attr->forecast_channels[i] - 1;
                    p_data[sample_data_len - p_algo_attr->data_dim + forecast_channel_idx] = p_forecasts[i];
                }
            }

            status = p_tss_task_ops->fc_ops.predict(p_data, p_forecasts);
            if (status != TSS_SUCCESS)
            {
                /* Handle the prediction failure cases */
            }

            recursive_cnt++;  
                
            /* Move the data window forward by one time step for the next recursive prediction */
            memmove(p_data, p_data + p_algo_attr->data_dim, sizeof(float)*(sample_data_len - p_algo_attr->data_dim));
            
            if (recursive_cnt == p_algo_attr->recursive_length)
            {/* Remark: The condition to end recursive forecasting can be customized */ 
                /* Handle the recursive forecasting ending case */
            }

            /* Handle the forecasting result */
        }
    }
    return 0;
}


Notes: The above example is a “Hello World” level code to illustrate the use of the algorithm library or binary for different tasks.


API Reference

Notes: The APIs are changed from v1.5 to support both library format and binary format.

Files

TimeSeries.h: The API header file for the library or binary, developers use it for the algorithm integration.

#include "TimeSeries.h"

Enumerations

name

description

typedef

tss_status

Status codes returned from functions in the library or binary

typedef

task_type_t

Algorithm task type

typedef enum
{
    TSS_SUCCESS                 = 0, /* No error */
    TSS_STATE_ERROR             = 1, /* State is incorrect */
    TSS_BOARD_ERROR             = 2, /* Board information is incorrect */
    TSS_MEMORY_ERROR            = 3, /* Memory error caused by the HEAP Overflow */
    TSS_PREDICT_NOT_ENABLED     = 4, /* Predict function is not enabled */
    TSS_LEARNING_ERROR          = 5, /* Errors occurs during the learning process */
    TSS_LEARNING_NOT_ENOUGH     = 6, /* Not enough calls to learning */
    TSS_RECOMMEND_LEARNING_DONE = 7, /* Reached the recommended calls to learning */
    TSS_NOT_READY               = 8, /* Function is not ready but planed to support */
    TSS_LICENSE_ERROR           = 9, /* Invalid license */
    TSS_UNKNOWN_ERROR           = 10, /* Unknown error */
} tss_status;

typedef enum {
    TASK_AD = 1,
    TASK_AD_ODL = 2,
    TASK_CLS = 3,
    TASK_OC = 4,
    TASK_REG = 5,
    TASK_FC = 6,
} task_type_t;

Structures

name

description

typedef

tss_algo_attribute_t

Algorithm attributes

typedef

tss_ad_task_ops_t

Operations for anomaly detection task

typedef

tss_ad_odl_task_ops_t

Operations for anomaly detection task with on-device-learning

typedef

tss_cls_task_ops_t

Operations for n-classification task

typedef

tss_oc_task_ops_t

Operations for one-class classification task

typedef

tss_reg_task_ops_t

Operations for regression task

typedef

tss_fc_task_ops_t

Operations for forecasting task

typedef

tss_task_ops_t

Task-specific operations union

typedef struct {
    unsigned int data_len; /* The length of the input data */
    unsigned int data_dim; /* The dimension of the input data */
    unsigned int model_size; /* The size of the model buffer */
    const float *model_addr; /* The address of model buffer that stores the model hyper-parameters */
    unsigned int target_num; /* The number of targets or classes */
    float recommend_threshold; /* The recommended threshold */
    const char *lib_id; /* Identifier for the library or binary */
    const char *neutron_version; /* The software version of neutron, if supported */
    unsigned int recommend_learning_num; /* The recommended number of learning */
    unsigned char odl_supported; /* On-Device-Learning is supported, or not */
    unsigned char neutron_enabled; /* Neutron is enabled, or not */
    unsigned char powerquad_enabled; /* PowerQuad is enabled, or not */
    unsigned char recursive_predicted; /* Recursive prediction is enabled, or not */
    unsigned int recursive_length; /* The length of the recursive prediction */
    unsigned int forecast_horizon_number; /* The number of forecast horizons */
    const unsigned int *forecast_horizons; /* The forecast horizons array */
    unsigned int forecast_channel_number; /* The number of forecast channels */
    const unsigned int *forecast_channels; /* The forecast channels array */
    float fbeta_beta; /* The beta value used for the Fbeta score */
    unsigned int fbeta_label_id; /* The label id used for the Fbeta score */
} tss_algo_attribute_t;

typedef struct tss_ad_task_ops
{
    /**
     * @brief      Initialize the anomaly detection algorithm.
     * @retval     TSS_SUCCESS              - Initialization succeed.
     */
    tss_status (*init)(void);

    /**
     * @brief      Predict the normal probability of the specified data.
     * @param[in]  data_input               - The data input for the prediction.
     * @param[out] probability              - The predicted probability output.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     * @retval     TSS_PREDICT_NOT_ENABLED  - Model not ready for prediction.
     */
    tss_status (*predict)(const float data_input[], float *probability);
} tss_ad_task_ops_t;

typedef struct tss_ad_odl_task_ops
{
   /**
    * @brief      Initialize the anomaly detection algorithm with the specified model.
    * @param[in]  model_buffer             - The model buffer for initialization, NULL means reset the model.
    * @retval     TSS_SUCCESS              - Initialization succeed.
    */
    tss_status (*init)(const float model_buffer[]);

    /**
     * @brief      Learn new model from the normal data.
     * @param[in]  data_input               - The data input for the learning.
     * @retval     TSS_SUCCESS              - Learning succeed
     * @retval     TSS_LEARNING_NOT_ENOUGH  - More data needed for the learning.
     */
    tss_status (*learn)(const float data_input[]);

    /**
     * @brief      Export the model to the specified buffer.
     * @param[out] model_buffer             - The exported model buffer.
     * @retval     TSS_SUCCESS              - Export succeed.
     * @retval     TSS_PREDICT_NOT_ENABLED  - Model not ready for export.
     */
    tss_status (*export_model)(float model_buffer[]);

    /**
     * @brief      Predict the normal probability of the specified data.
     * @param[in]  data_input               - The data input for the prediction.
     * @param[out] probability              - The predicted probability output.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     * @retval     TSS_PREDICT_NOT_ENABLED  - Model not ready for prediction.
     */
    tss_status (*predict)(const float data_input[], float *probability);
} tss_ad_odl_task_ops_t;

typedef struct tss_cls_task_ops
{
    /**
     * @brief      Initialize the classification algorithm.
     * @retval     TSS_SUCCESS              - Initialization succeed.
     */
    tss_status (*init)(void);

    /**
     * @brief      Predict the probabilities and class index of the specified data.
     * @param[in]  data_input               - The data input for the prediction.
     * @param[out] probabilities            - The predicted probabilities of all classes
     * @param[out] class_index              - The predicted class index.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     */
    tss_status (*predict)(const float data_input[], float probabilities[], int *class_index);
} tss_cls_task_ops_t;

typedef struct tss_oc_task_ops
{
    /**
     * @brief      Initialize the one class algorithm.
     * @retval     TSS_SUCCESS              - Initialization succeed.
     */
    tss_status (*init)(void);

    /**
     * @brief      Predict if is outlier and the decision score of the specified data.
     * @param[in]  data_input               - The data input for the prediction.
     * @param[out] is_outlier               - The predicted results of if input is outlier.
     * @param[out] score                    - The predicted score.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     */
    tss_status (*predict)(const float data_input[], float *score, int *is_outlier);
} tss_oc_task_ops_t;

typedef struct tss_reg_task_ops
{
    /**
     * @brief      Initialize the regression algorithm.
     * @retval     TSS_SUCCESS              - Initialization succeed.
     */
    tss_status (*init)(void);

    /**
     * @brief      Predict the targets based on the specified data.
     * @param[in]  data_input               - The data input for the prediction.
     * @param[out] targets                  - The predicted targets output.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     */
    tss_status (*predict)(const float data_input[], float targets[]);

} tss_reg_task_ops_t;

typedef struct tss_fc_task_ops
{
    /**
     * @brief      Initialize the forecasting algorithm.
     * @retval     TSS_SUCCESS              - Initialization succeed.
     */
    tss_status (*init)(void);

    /**
     * @brief      forecast the targets based on the specified data.
     * @param[in]  data_input               - The data input for the forecasting.
     * @param[out] forecasts                - The forecasted output.
     * @retval     TSS_SUCCESS              - Prediction succeed.
     */
    tss_status (*predict)(const float data_input[], float forecasts[]);

} tss_fc_task_ops_t;

typedef struct tss_task_ops
{
    int task;
    union
    {
        tss_ad_task_ops_t ad_ops;
        tss_ad_odl_task_ops_t ad_odl_ops;
        tss_cls_task_ops_t cls_ops;
        tss_oc_task_ops_t oc_ops;
        tss_reg_task_ops_t reg_ops;
        tss_fc_task_ops_t fc_ops;
    };
    const tss_algo_attribute_t *(*algo_attribute)(void);

} tss_task_ops_t;

Functions

The generated algorithm provides the following main functions:

tss_get_task_ops()

const tss_task_ops_t* tss_get_task_ops(void);

Description: Returns a pointer to the task operations structure for the generated library.

Returns: Pointer to tss_task_ops_t structure containing task-specific operations and attributes.

Usage: This is the primary entry point for library format integration. Call this function during initialization and obtain access to all algorithm operations.

Example:

const tss_task_ops_t *p_tss_task_ops = tss_get_task_ops();
if (p_tss_task_ops == NULL) {
    // Handle error
}

Task-Specific Operations

Based on the task type, access the appropriate operations through the returned structure:

  • Anomaly Detection: p_tss_task_ops->ad_ops

  • Anomaly Detection with ODL: p_tss_task_ops->ad_odl_ops

  • Classification: p_tss_task_ops->cls_ops

  • One-Class Classification: p_tss_task_ops->oc_ops

  • Regression: p_tss_task_ops->reg_ops

  • Forecasting: p_tss_task_ops->fc_ops

algo_attribute()

const tss_algo_attribute_t* (*algo_attribute)(void);

Description: Retrieves algorithm attributes including data dimensions, model size, and hardware acceleration status.

Returns: Pointer to tss_algo_attribute_t structure.

Example:

const tss_algo_attribute_t *p_algo_attr = p_tss_task_ops->algo_attribute();
printf("Data length: %u, Data dimension: %u\n", 
       p_algo_attr->data_len, p_algo_attr->data_dim);

Algorithm Project Execution

eIQ Time Series Studio helps generate the sample project, which can be directly imported in the MCUXpresso IDE. The sample project contains a generated algorithm library or binary, time series framework, your target project driver, settings, and components. You can take the sample project as a QuickStart with your own library or binary.

Sample project workflow overview:

alt text

  • Idle state. Ready to handle the SHELL commands and collect the sensor data by the sensor HAL in time series framework.

  • Data log state. Print the sensor data via SHELL over UART.

  • Prediction state. Predict based on the sensor data by the generated model algorithm and print the results via SHELL over UART.

  • On-device-Learn state. Learn a new model from the sensor data by the generated model algorithm and print the results via SHELL over UART.

Sample Projects key features:

  • QuickStart with your algorithm on the target Edge device.

  • User-friendly SHELL in the serial terminal, start the learning/prediction process with commands.

  • Provides an option to log the data when the target has an embedded sensor (accelerator).

  • To test the algorithm without a physical sensor as the data input, use a dummy sensor HAL in the Time Series framework.

Based on the MCX-N9XX-EVK, the file tree of the generated sample project is shown as below.

    📦MCX-N9XX-EVK <Debug_lib>       Choose the build option for project with library or binary.
    ┣ 📂Framework                    time series framework based on the FreeRTOS.
    ┃ ┣ 📂core
    ┃ ┣ 📂docs
    ┃ ┣ 📂hal                        Hardware Abstraction Layer.
    ┃ ┃ ┣ 📂inc
    ┃ ┣ 📂inc
    ┗ 📂MCX-N9XX-EVK                 Base Project.
    ┃ ┣ 📂CMSIS
    ┃ ┣ 📂board
    ┃ ┣ 📂component
    ┃ ┣ 📂device
    ┃ ┣ 📂drivers
    ┃ ┣ 📂freertos
    ┃ ┣ 📂source
    ┃ ┃ ┣ 📂TimeSeries              Generated time series library or binary.
    ┃ ┃ ┣ 📜FreeRTOSConfig.h        FreeRTOS config header file.
    ┃ ┃ ┣ 📜cpp_config.cpp
    ┃ ┃ ┣ 📜hardware.c              Config file of the hardware/sensors.
    ┃ ┃ ┣ 📜lptmr.c
    ┃ ┃ ┣ 📜lptmr.h
    ┃ ┃ ┣ 📜main.c                  Main program.
    ┃ ┃ ┣ 📜memory.c
    ┃ ┃ ┗ 📜semihost_hardfault.c
    ┃ ┣ 📂startup
    ┃ ┣ 📂usb
    ┃ ┣ 📂utilities
    ┃ ┣ 📜.cproject
    ┃ ┣ 📜.gitignore
    ┃ ┣ 📜.project
    ┃ ┗ 📜README.pdf                User Guide of the sample project.

SHELL Interface

After clicking GENERATE with the project option and completing the build-flash steps, the time series sample project flashes directly into your device. Open the Serial Terminal and start the execution:

alt text

The command-line interface is straightforward as reflected in the output from help:

"help": List all the registered commands

"exit": Exit program

"start <log|learn|pre>: Start an execution
- log: Start data logger
- learn: Start time series learning
- reset: Start time series knowledge reset
- pre: Start time series prediction

"stop": Stop ongoing execution

"setup <odr|fsr|sc|thold> <value>: Setup a parameter
- odr: Setup output data rate
- fsr: Setup full scale range
- sc: Setup sample count
- thold: Setup prediction threshold (Anomaly Detection Only)

"loadlib <load|alloc> <allocsize | line>: dynamic load a library to allocated memory
- alloc size: allocate memory of size bytes
- load line: load one line of library to memory

"get <info|state|range>: Get board information
- info: Get system information
- state: Get current Time Series state
- range: Get parameter range

Button interface

To execute the “start pre”, “start learn”, and “stop” of shell instructions, the sample project supports a simple button interface 🔘 on the board.

  • If there is a support for two buttons on the board, toggling them means toggling “start pre/stop”, and “start learn/stop”.

  • If there is support for only one button, toggling means “start pre/stop”.

  • If the prediction or learn or data log is ongoing, press any supported button stops the execution.

🏆 Congratulations!

You have completed the whole process from the data import to the final algorithm library or binary generation. You can now proceed with the time series AI/ML algorithm deployment for your real device.