Training

Switch to the Training tab after loading the datasets. The training function is the core technology, including data preprocessing, automation for algorithm hyperparameter searching, benchmark testing, and optimal accuracy fitting optimization for limited flash and RAM size. Model performance can also be evaluated through various benchmark indicators.

Function Layout

The following figure shows the layout of the Training tab, which is divided into several parts: Training Records, Models, Training Info, Benchmark, Training Curve, Validation Results, Confusion Matrix, and Statistic Data.

image

The Training Records part records all the training tasks created by the user.

The Models part records all the models generated from a specific training task. The models are sorted in descending order of their score. The score depends on the size of RAM/flash usage and some common evaluation metrics shown in Benchmark.

The Training Info records the training time, progress, and configuration information; including date, version, model type, max RAM, max flash, quick search, on-Device learn (for anomaly detection), train/validation ratio and data used for training.

The Training Curve records the change curves of balanced accuracy, flash, and RAM used with auto machine learning. The same horizontal axis represents the balanced accuracy, flash, and RAM used of the specific model.

The Validation Results part shows the validation results of the selected model on the validation dataset.

The Confusion Matrix displays a matrix showing the predicted labels versus actual labels, helping to visualize model performance.

The Statistic Data part provides detailed statistical metrics and performance indicators for the selected model and training task.

In general, there are five types of tasks that support time series-based dataset applications, which are anomaly detection, n-class classification, 1-class classification, regression and forecasting. The information in the right frame varies with different task types. The task types are introduced in detail in the subsequent content.

Anomaly Detection

Algorithm Benchmark:

image
  • BALANCED ACCURACY: Average accuracy is obtained from both the minority and majority classes.

  • F1: The F1 score is a metric that reflects the global performance of a classifier, the value ranges from 0 to 1.

image
  • RECALL: The recall is intuitively the ability of the classifier to find all the positive samples, the value ranging from 0 to 1.

image
  • FLASH: Minimum flash size required for selected algorithm.

  • RAM: Minimum RAM size required for selected algorithm.

  • Execution Time: The estimated time for one inference in the algorithm library, using the LPC55S36 platform (Cortex-M33, 150 MHz, with hard float-point enabled).

At the same time, you can get the execution time by clicking the clock button.

Algorithm Validation Results:

image

During the training, a part of the data is used for validation from time to time. The training curve reflects those results as the metric of accuracy for the result.

  • The x-axis means the validation sample index. (For anomaly detection, all samples are used for validation, while classification validates samples according to Train/Val Ratio.)

  • The y-axis means the probability, which normalized from 0 to 1.

  • The green points are true positive/negative and the red points are false positive/negative.

Learning Curve:

For models that support On-Device Learn, learning curves are provided, showing the effect of adding more samples during training.

image

Confusion Matrix:

For anomaly detection, the confusion matrix table contains normal and anomaly results, see the chart below.

image

You can also get the percentage results by clicking the percent(%) button.

image

You can also view the statistical results.

image

n-Class Classification

Algorithm Benchmark:

For classical machine learning in n-class classification tasks, some evaluation metrics are consistent with anomaly detection, such as balanced accuracy, RAM, flash, and F1.

image

When you enable Optimize for a specific class (Fβ) in the training configuration, an additional Fβ metric is shown in the benchmark. Its header indicates the configured β value and the target class (for example, Fβ (β=0.5, Empty)).

image
  • Fβ: The Fβ score is the weighted harmonic mean of precision and recall for the selected target class, the value ranges from 0 to 1. β is a positive value (greater than 0): β greater than 1 favors recall, β less than 1 favors precision, and β equal to 1 is equivalent to the F1 score.

image
  • ROC_AUC: ROC_AUC is the area under the receiver operating characteristic curve, the value ranges from 0 to 1.

Unlike classical machine learning, deep learning models quantify the memory requirements using parameters, such as Algorithm Buffer and Model Size.

image
  • Algorithm Buffer: Buffer estimated for signal processing and inference together.

  • Model Size: The size of deep learning model for weights and bias.

Algorithm Validation Results:

For n-class classification, validation results are displayed similarly to anomaly detection, showing the performance of the model across all classes during training.

image

Confusion Matrix:

For n-class classification tasks, the confusion matrix table rescales to fit all classes, see the chart below.

image

Statistic Data:

For n-class classification tasks, statistical results for all classes can be viewed.

image

Threshold:

For n-class classification tasks, a Threshold is provided for re-evaluating the performance of the models. The models are reranked according to the balanced accuracy after setting the Threshold.

image

After setting the threshold, a line with the threshold appears in the validation results view. The results with a probability less than the set threshold are re-evaluated as uncertainty.

image

At the same time, the statistic data is updated accordingly.

image

1-Class Classification

As a special case of classification, 1-class classification only has recall as the main evaluation metric because of lack of negative samples.

image

And the validation results chart is not the confusion matrix but the distance to the decision boundary.

image

Regression

Algorithm Benchmark:

For classical machine learning in regression tasks, benchmark information includes R2, RAM, flash, and Execution time.

image
  • R2: The coefficient of determination. The formula is available in the regression emulation metric section.

  • FLASH: Minimum flash size required for selected algorithm.

  • RAM: Minimum RAM size required for selected algorithm.

  • Execution Time: The estimated time for one inference in the algorithm library, using the LPC55S36 platform (Cortex-M33, 150 MHz, with hard float-point enabled).

Like n-class classification tasks, deep learning models quantify the memory requirements using parameters, such as Algorithm Buffer and Model Size.

image

Algorithm Validation Results:

image

The predicted values of each regression target for all validation samples are plotted.

  • The x-axis means the validation sample index. Train/Val Ratio validates the number of samples used for validation.

  • The y-axis means the predicted value.

  • The dotted line represents the true value.

Evaluation Matrix:

image
For regression, the values of MSE, RMSE, MAE, R2, and SMAPE for all regression targets are given including the average of these values.
  • MSE: The mean square error.

image
  • RMSE: The root mean square error.

image
  • MAE: The mean absolute error.

image
  • R2: The coefficient of determination.

image
  • SMAPE: The symmetric mean absolute percentage error.

image

*Notes: In the formulas, Xi is the predicted ith value. The Yi element is the actual ith value. The regression method predicts the Xi element for the corresponding Yi element of the ground truth dataset. Reference comes from [the coefficient of determination R-squared is more informative than SMAPE, MAE, MAPE, MSE, and RMSE in regression analysis evaluation.]

Forecasting

Algorithm Benchmark:

For forecasting tasks, benchmark information includes MAE, RAM, flash, and Execution Time.

image
  • MAE: The horizon-aware mean absolute error. It is a weighted result across the forecasting horizon (steps): the smaller the horizon (the nearer the step-ahead position), the larger its weight, so near-term predictions contribute more to the final score than far-term predictions. The base MAE formula is available in the regression emulation metric section.

  • FLASH: Minimum flash size required for selected algorithm.

  • RAM: Minimum RAM size required for selected algorithm.

  • Execution Time: The estimated time for one inference in the algorithm library, using the LPC55S36 platform (Cortex-M33, 150 MHz, with hard float-point enabled).

Algorithm Validation Results:

image

The predicted time series is plotted against the validation time series for each forecasting target and recursive step-ahead (for example, Channel_1_1_ahead).

  • The x-axis means the time index.

  • The y-axis means the value of the target channel.

  • The Validation Data series represents the true value, and the Predicted series represents the forecasted value.

  • Use the Recursive Step and Step selectors to switch between different step-ahead predictions.

Evaluation Metrics:

image

For forecasting, the values of MAE, RMSE, and SMAPE are given for each target channel (for example, Channel_1_1_ahead), along with an OVERALL row that averages these metrics across all targets. The definitions of MAE, RMSE, and SMAPE are available in the regression emulation metric section.

Training Process

This section introduces how to start, pause, stop, and manage training.

Start New Training

Click the Start New Training button.

If this is your first time training, a Training Config pop-up appears. Refer to the New Training section below for detailed configuration instructions.

If you already have trained models for your project, a Select Training Type pop-up appears. It includes two options:

  • New Training

  • Use Trained Model

If you select New Training, the process is the same as your first-time training. Refer to the New Training section for configuration details.

If you select Use Trained Model, refer to the Use Trained Model section below for detailed configuration instructions.

image

New Training

Click New Training button, and a pop-up box appears for configuration. You can rename the training in the Name box. Before you click the Start button, check the feasible options to configure for the different algorithm tasks. Usually, you can go for training without changing the configuration and get the best result.

Classical Machine Learning (CML) Configuration

Some configuration options are shared across tasks. They are described once here and are not repeated for each task below:

  • CML — Choose to train the CML models.

  • DL — Choose to train the DL models. (Availability depends on the task; see the Deep Learning (DL) Configuration section for the DL-specific options.)

  • Quick Search — Speed up the training in a small search space. The search scope of this mode is not as large as the default mode.

  • Train/Val Ratio — Adjust the ratio of training and validation data (for example, 8:2).

The remainder of this section highlights only the options that are specific to each task.

The following is the configuration option for anomaly detection.

image

The anomaly detection algorithm is based on semi supervised machine learning that supports on-device training.

  • Supports both CML and DL models. For the DL-specific options, see the Deep Learning (DL) Configuration section.

  • On-Device Learn applies to CML models. If the algorithm is for prediction only, do not enable On-Device Learn. This action results in a larger RAM/flash size.

  • If the dataset in use has variations, you can enable On-Device Learn to support on-device training.

  • If you want to get training results quickly, enable Quick Search. The search scope of this mode is not as large as the default mode.

The following are configuration options for classical machine learning in classification tasks:

image

In addition to the shared options above, the classification task provides:

  • Advanced Training Configs:

    • Optimize for a specific class (Fβ) — Enable to optimize the model toward a specific class using the Fβ score.

      • Target Class — Select the class to optimize for (for example, Empty).

      • β — Set the Fβ weight. A value greater than 1 favors recall, less than 1 favors precision, and 1 equals the F1 score.

The following are configuration options for classical machine learning in 1-class classification tasks. The 1-class classification task uses only the shared options described above (CML, DL, Quick Search, and Train/Val Ratio).

image

The following are configuration options for classical machine learning in regression tasks:

The Shuffling Data option is enabled by default to improve model generalization. You can disable it if your dataset has a specific order that must be preserved.

image

The following are configuration options for classical machine learning in forecasting tasks. The forecasting task supports only CML models (DL is not supported), together with the shared Quick Search and Train/Val Ratio options:

image

In addition to the shared options above, the forecasting task provides:

  • Lookback — Determines how many historical observations are used as input. It should be large enough to cover the potentially informative lags. (Users can either define this value based on their forecasting scenario or refer to the recommended lookback derived from dataset analysis.)

  • Stride — Determines how many time steps the sliding window advances between samples. (Smaller values create more overlapping samples; larger values reduce dataset size.)

  • Recursive Length — Number of recursive prediction iterations performed during training. (Applicable only when recursive forecasting is enabled)

Deep Learning (DL) Configuration

The following are the configuration options for deep learning tasks. The screenshots below illustrate the configurations on both Windows and Linux platforms. You can select a specific deep learning model to train:

image
image 2

Deep learning models support user-defined hyperparameter settings. Detailed information about the supported hyperparameters is presented in the tables below.

Important: Larger batch sizes require more GPU memory and may lead to out-of-memory (OOM) errors during training. To ensure stable training, start with a smaller batch size (for example, 16) and increase it gradually based on the available GPU resources and model requirements.

image 2
image 2

As for GPU acceleration, you can enable GPU to speed up the training process if your system has a compatible GPU available. Disabling GPU uses CPU-based training instead.

Use Trained Model

When you select the Use Trained Model option, you can start a new training based on previously trained models within your project. Internally, our training engine parses the selected models and uses their existing knowledge to build a more specialized model for the new training.

Compared to the New Training option, this approach builds upon prior model knowledge, which can potentially reduce both training time and computational resource usage.

This option is especially useful when you have only updated the training dataset since the last training and want to generate new models.

image

Common Options:

  • Configure Train/Val Ratio, change with a different ratio if the train/emulation accuracy mismatches or is out of range.

After the training configuration is done or the settings are set to default, click the Start button. Wait until the training is complete. The time to complete the training depends on the following factors:

  • The size of the dataset.

  • The type of algorithm task you choose.

  • Different training configurations can also result in different time costs.

Once training is complete and satisfactory results are achieved, you can review the results.

When training starts, the training progress bar is continuously updated, and the timer keeps counting until all content is 100 % complete.

image

Pause/Stop Training

During the training process, you can choose to click the Stop button to stop the training or click the Pause button to pause the training.

image

After the pause, you can view the training results of any model in the model list on the left. Alternatively, you can click the Resume button to continue the training.

image

Training Record Management

As shown in the figure below, after tasks are completed, all training records appear. The candidate algorithm list appears and is sorted by performance. The pattern C indicates that the record was trained using classical machine learning models, and the pattern D indicates using deep learning models.

image 1 image 2

To view or download the flowchart and report of the corresponding model for further reference, click the flowchart and report buttons.

image
image

Click and choose any of the algorithm results from the list and get the benchmark details as below. In the Training diagram, the purple arrow coordinates indicate the currently selected model. You can also view the auto machine-learning training curve and the balanced accuracy, flash, and RAM corresponding to each model.

image

In addition, you can also delete the corresponding training record by clicking the Delete button. After deletion, all model information under the training record will be deleted at the same time.

image

Model List and Code License

To keep the algorithm transparent as required by customers, we keep the list of all supported models updated according to the release version.

Classical Machine Learning Model List

image

Deep Learning Model List

image

The table highlights the following information:

  • Models for each task.

  • Python code source, which used for training.

  • Python code license type.

  • C code source, which used for deployment.

  • C code license type.