Data Labeling

The Data Labeling Tool provides a visual interface that allows users to categorize imported raw data. Tags such as arc or no-arc, and snoring or no-snoring can be applied to specific sections of the graph. This tool then segments the raw data based on labeling and creates datasets optimized for training machine learning models. We also provide a prelabeling tool to assist with labeling (optional).

Click the Data Labeling button under the Utilities set to open Data Labeling tool.

Entry

Data Import

Raw data: Continuous current data is stored in time sequence. It is single-channel data, in CSV format (values separated by spaces) or float32 WAV format (single channel).

Import data

CSV Data Import

If your data is in CSV format, an additional import settings panel will appear when you select a CSV file. Enter the sample rate (which can also be modified after importing) and select a data format from the list.

CSV Import Settings CSV Import Settings

The available data formats are:

  • Normalize: Raw unnormalized data that will be normalized to float32 in the range [-1, 1].

  • int16: int16 format.

  • int32: int32 format.

  • float32: Normalized float32 format, range [-1, 1].

If multiple files are imported at once, these settings will be applied to all files in the batch.

Edit Sample Rate

To edit the frequency of a data file (optional):

  1. Select the target file in the file list on the left, then click the Edit button.

    Edit Frequency Edit Frequency 1

  2. Enter the frequency value, then click the check button to apply the change.

    Edit Frequency 2

Labeling

Rename Labels

The label list contains labels for classification. The number of labels in the list corresponds to the number of classes. When you first access this tool, the label list is empty. Click the + button, create a class, and add it to the label list.

Empty labels

Add class 1

You can edit the alias of labels. This operation is optional and only intends to enhance label readability.

  • To edit the alias, first click the edit button:

Rename class 1

  • Second, input the alias string, then click the check button to apply the rename.

Rename class 2

To rename all labels one by one, repeat the steps above.

Rename class 3

Labeling Operations

Overview

  • Waveform: Time series waveform of data.

  • Spectrogram: Time-frequency domain waveform of data, using STFT transform. The horizontal axis represents time, while the vertical axis represents frequency.

  • Labeled region list: Each region drawn on the time series waveform corresponds to a record here, including the classification label, start time, and end time.

  • Step 1: Select a file to label.

    Select a file

  • Step 2: Draw a range on a waveform graph.

    Labeling

  • Step 3: Choose the label for the labeled region.

  • Repeat steps from 2 to 3 and label all the regions.

  • Repeat steps from 1 to 3 to label all data files.

    labeled all

Edit Labeled Result

Edit region: You can modify the range of a region by dragging its boundaries.

Edit Region

You can change the label of a region by reselecting it.

Note: All ranges must be labeled before running the data generation.

Generate Dataset

Generate Dataset

Click the Generate Dataset button. After processing, the data folders, segmented according to the labeling results, appear in a pop-up window.

Dataset

Note: You can import the segmented data into Data Intelligence to analyze and obtain the recommended parameters such as window size, sample frequency. Next, use Data Operation to process the segmented continuous data according to the recommended parameters to create a dataset suitable for training.

Prelabeling (Optional)

We provide a prelabeling tool that can automatically perform prelabeling on continuous data. You can make adjustments based on the prelabeling results to reduce the labeling workload.

Prelabeling button

To use prelabeling:

  1. Import your continuous data files. Here we load an audio file containing snoring sounds to demonstrate the snoring detection prelabeling process.

    File import

  2. Click the Pre-labeling Tool button. In the pop-up window, select a prelabeling algorithm (which currently only supports the snoring detection algorithm). Click the Confirm button and confirm your selection.

    Algorithm selection

    A warning dialog pops up, stating that this operation deletes all previous results. If you want to proceed, click the Confirm button and enter the prelabeling process panel.

    Confirm warning

    The label list is automatically changed to the preset of the algorithm.

    Prelabeling label list

  3. Configure the parameters of the prelabeling algorithm. The number and type of parameters depend on the prelabeling algorithm selected. Different algorithms have different parameters or use the default values. Select the file list that needs prelabeling (must be files that have already been imported). Next, click the Apply button, and click Confirm on the warning dialog that appears. Wait for a moment to complete the prelabeling process.

    Config prelabeling

    Writing prelabeling

  4. The prelabeling results appear in the labeled region list. Review all results and manually adjust the window or label categories, delete or add regions as needed. The subsequent process is the same as the standard manual labeling workflow.

    Prelabeling results