Projects

The Projects page enables you to configure specific settings for your projects. The settings are slightly different for different tasks. Also, the BYOD projects are supported across all tasks, while the BYOM projects are currently available only for the n-class classification and regression tasks. The following sections provide the steps to configure settings for anomaly detection, classification, regression, and forecast.

Anomaly Detection

image

On the Projects page of Anomaly Detection, there are six settings to configure. These settings include Project Name, Your Target, Library Max RAM, Library Max Flash, Description, Sensor Configuration. The settings appear on the click of the Create New Project button.

In Project Name, users must assign a unique name of their project. If the name is the same as an existed project name, users are unable to create a project.

image image

In Your Target, you can select the board on which you want to deploy the trained model. The supported boards are all included in the drop-down list in the figure shown above. You could also view the resource information of selected boards, such as the CPU core frequency.

After the target board selection, Library Max RAM and Library MAX Flash are automatically set to the default values of the selected board. For example, the Library Max RAM and the Library Max Flash are set to 512 kB and 2048 kB when the target board is FRDM-MCXN9XX. Moreover, you can also customize the values of the Library Max RAM and the Library Max Flash. Larger values indicate a larger search space in the training stage, and intend to achieve higher accuracy in the target task. Smaller values generate resource-friendly models, which have small RAM/Flash size. Also, Library Max RAM and the Library Max Flash are not constrained when the set as 0.

In Description, you can provide some explanations or leave it blank.

image

In Sensor Configuration, you must set sensor types and the number of channels of the input signal. Once you configure and save, you cannot change this parameter in a project. For example, in the Sample App Arc Detection of anomaly detection, the input signal consists of a channel of current signal. Therefore, the sensor type of Current is selected from the drop-down list for channel 1. If the sensor type of the signal is not known, you can choose Generic from the drop-down list.

After configuring all these settings, click the Confirm & Create button to proceed the following steps.

Besides, you can also import an existing eIQ Time Series Studio project by clicking the Import button. The imported project has the same configuration as the original project.

n-Class Classification

For n-class classification tasks, users can create either a BYOD project or a BYOM project by clicking the corresponding button: BYOD Project or BYOM Project. A BYOD Project enables users to experiment with various combinations of signal processing pipelines and machine learning models. In contrast, a BYOM project allows users to bring their own pretrained deep learning models, eliminating the need to train models from scratch.

image image

After clicking the button of BYOD Project or BYOM Project, users have seven settings to configure for the desired project. Six out of seven settings are similar to the anomaly detection settings. However, you must configure the Number of Classes for classification projects. For example, in the Sample App Human Activity Recognition of classification, the project searches a model to distinguish six activities. The activities are downstairs, upstairs, walking, jogging, sitting, and standing. Therefore, for this project, the value of Number of Classes is set to 6. Once you configure and save, you cannot change this parameter in a project.

Also, the values of Library Max RAM and Library Max Flash do not take effect on BYOM projects. The values are provided solely as reference to help ensure your model fitted within memory constraints during deployment.

1-Class Classification

Similar to multiclass classification, 1-class classification projects can be created as BYOD projects. However, 1-class classification focuses on detecting anomalies or outliers within a single class of data. In this scenario, no Number of Classes parameter is required. The class number defaults to 1.

Regression

For regression tasks, users can also create either a BYOD project or a BYOM project by clicking the button of BYOD Project or BYOM Project.

image image

After clicking the button of BYOD Project or BYOM Project, there are seven settings to configure on the Projects page of regression. Six out of seven settings are similar to the anomaly detection or classification settings. However, you must configure the Input/Output Targets for regression projects. The Input/Output Targets indicates the number of targets of a regression model. For example, in the Sample App Electric Motor Temperature of regression, the project predicts the temperature and the torque of the motor. Therefore, the Input/Output Targets is set to 2. Similar to the Number of Classes, once you configure and save, you cannot change this parameter.

Similar to classification tasks, the values of Library Max RAM and Library Max Flash do not take effect on the BYOM project. These values are provided solely as reference to help ensure your model fitted within memory constraints during deployment.

Forecast

For forecast tasks, users can create a BYOD project by clicking the BYOD Project button. Forecast projects include four settings that differ from those of other tasks. A brief guide to configuring these settings is provided below.

image image
  • Cross Instance: Use this toggle to control whether the forecast model can learn across different instances in the dataset.

  • Forecast parameters

    • Recursive: Use this toggle to control whether the forecast model uses recursive multi-step forecasting. When Recursive is enabled, Forecast Horizons is set to 1 and cannot be changed.

    • Forecast Horizons: Specify the expected values for Forecast Horizons. You can enter comma-separated values or ranges, for example, 1,3,5 or 1-10.

    • Forecast Channels: Specify which channels you want the model to forecast.